pix vertUpdate: 21/07/2008
      Back to Home
         

The "Energy Efficiency" label has been designed to help you make a focus on the EE outline you develop in any communication tool.

It is part of our identity: do not modify!
 
Old versions!





Do not use anymore!
       
       
pix vertEnergy Efficiency Solutions
pix vert
       

For generic use, we suggest to use the "up to 30% energy saving" label associated with the following sentence: "30% saving is feasible today with existing technologies."
 
       

For specific values *
This "Energy Efficiency label" is to be associated to descriptions of solutions.

* The percentage is the expected potential energy saving of the solution you emphasis on.
 
pix vert    
         
pix vertBenefit
     
pix vertThanks to these labels you can highlight the Energy Efficiency benefit and make the difference compared to a traditional solution.      
         
         
pix vertVariations and downloads
pix vert
         
pix vert  
Download EE_labels_02 files

Download EE_labels_03 files
Each downloaded Zip file contains the 3 versions of EE label.
(Adobe Illustrator files)
         
         
pix vert       
Download EE_labels_01 files
         
         
pix vert
Download EE_label_Black files
for Black and white applications
    
Download EE_label_White files
for single colour applications
         
         
pix vertAll information has been validated by Corporate Communication.
pix vert© 2009 / Schneider Electric Industries SAS. All rights reserved.